{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the lug wire range for the SN1200 neutral assembly?
Issue:
Product Features

Product Line:
Circuit Breaker Enclosure Accessory

Resolution:
The standard lugs provided on the neutral assembly will accept (4) #3/0 AWG - 750 kcmil Cu/Al conductors, incoming and outgoing. However, the P frame enclosures are marked for use with 500 kcmil conductors maximum, so this would restrict the neutral conductors also to 500 kcmil maximum.

Schneider Electric USA