{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Which Modbus programming cable do I need to communicate with a Compact 984 controllers?
Issue
Programming cable for Compact 984

Product Line
Compact 984

Resolution
If you're using Compact A984 or E984-241/245/251/255 PLCs, you will need a Modbus serial AS-W952-012 programming cable.

If you're using Compact E984-258/265/275/285 PLCs, you will need the following two items to communicate to this PLC:
110XCA28202.....10 ft. RS-232 communication cable assembly (with RJ45 connectors).
110XCA20300.....RJ45 to 9 pin female D-shell adapter.

The latest programming software that was sold for this by Schneider Electric was ProWORX 32. 
It was also programmed with the older ProWORX versions and Modsoft.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: