Issue: What is the pull apart terminal blocks and Din rail for a Model 6 MCC bucket ? Product Line: Model 6 MCC Environment: Maintenance Cause: Replacement Resolution: The Pull apart terminal blocks (5 Max per Din rail) is part number 80420-960-50 (each) and the Din rail is part number 80420-839-50 Note attached drawing , DIN Rail is 8.60" Long |
Released for:Schneider Electric USA
Issue:
What is the pull apart terminal blocks and Din rail for a Model 6 MCC bucket ? Product Line: Model 6 MCC Environment: Maintenance Cause: Replacement Resolution: The Pull apart terminal blocks (5 Max per Din rail) is part number 80420-960-50 (each) and the Din rail is part number 80420-839-50 Note attached drawing , DIN Rail is 8.60" Long |
Released for:Schneider Electric USA