Issue
Need to know the maximum number of concurrent Ethernet connections that the Powerlogic EGX150 supports
Product Line
EGX150
Environment
EGX150 Ethernet Gateway
Cause
Supported TCP/IP concurrent connections supported by the EG150
Resolution
The Powerlogic EGX150 is a Modbus to Ethernet gateway that can support a maximum of 16 concurrent Ethernet (Modbus TCPIP) connections.
Need to know the maximum number of concurrent Ethernet connections that the Powerlogic EGX150 supports
Product Line
EGX150
Environment
EGX150 Ethernet Gateway
Cause
Supported TCP/IP concurrent connections supported by the EG150
Resolution
The Powerlogic EGX150 is a Modbus to Ethernet gateway that can support a maximum of 16 concurrent Ethernet (Modbus TCPIP) connections.
Released for:Schneider Electric USA
Issue
Need to know the maximum number of concurrent Ethernet connections that the Powerlogic EGX150 supports
Product Line
EGX150
Environment
EGX150 Ethernet Gateway
Cause
Supported TCP/IP concurrent connections supported by the EG150
Resolution
The Powerlogic EGX150 is a Modbus to Ethernet gateway that can support a maximum of 16 concurrent Ethernet (Modbus TCPIP) connections.
Need to know the maximum number of concurrent Ethernet connections that the Powerlogic EGX150 supports
Product Line
EGX150
Environment
EGX150 Ethernet Gateway
Cause
Supported TCP/IP concurrent connections supported by the EG150
Resolution
The Powerlogic EGX150 is a Modbus to Ethernet gateway that can support a maximum of 16 concurrent Ethernet (Modbus TCPIP) connections.
Released for:Schneider Electric USA