{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the maximum number of devices that can be added in Com'X 510/200/210?
Issue
User wants to know how many devices can be added in the Com'X 510/200/210.

Product Line
Com'X 510 (EBX510)
Com'X 210 (EBX210)
Com'X 510 (EBX200)

Environment
Adding devices via the Webpage

Resolution
The Com'X 510/200/210 gateways support a total up to 64 devices with a maximum of 20 Modbus serial slave devices.

Schneider Electric USA