{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can NQFTL2H be used on 30 and 42 space interiors which normally use NQFTL2L?
Issue:
Can NQFTL2H be used on panelboards normally using NQFTL2L?

Product Line:
Panelboards.

Environment:
NQ

Cause:
Part NQFTL2L is not available, looking for a subsitute.

Resolution:
Yes, the NQFTL2H can be used on 30 and 42 curcuit interiors.  It will come with an extra piece of sheet metal that the contractor can throw away.

Schneider Electric USA