{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: How to manually trip a solid state Motor Logic™ Overload Relay
Issue:
Need to test manually SSOLR 9065

Product line:
NEMA and Definite Purpose Contactors and Starters

Environment:
NEMA Contactors and Starters Accessories 9065

Resolution:
Look on the under side of the unit for an indentation with an exposed opening that has a white plastic piece. Take a small screw driver and lift up that piece moving it to the right. You should hear a click. Check the front of the unit for the trip status indication, it should now indicate that it has been tripped. To reset the unit, press the red reset bar on the front of the overload relay device.

Schneider Electric USA