{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
PM5000 LE driver for ION enterprise 6.0 SP1
Issue
PM5000 series meters are not native supported on ION Enterprise 6.0 SP1 software.

Product Line
PM5000 series meters

Environment
ION Enterprise 6.0 SP1

Resolution
LE driver for PM5000 meters on ION Enterprise 6.0 SP1 attached to this article: Note: ION Enterprise 6.0 SP1 is no longer supported.

Run the "PM5000 LE 6.0.1.11 Driver Setup.exe" file inside the zip, and follow the installation process.  Once completed, The PM5000 series LE will be available when adding the device in the Management Console as a Device Type.  Add the PM5000 and verify connection.  If the newly added PM5000 meter values are not showing on Vista, perform a server restart.


NOTE: this driver is a LE (Limited Edition) driver. The LE driver supports all real time data registers, default PC logging but doesn't support retrieval of onboard logs or any digital output control operations. The PM5000 series meter is fully supported on the newer version of the software, Power Monitoring Expert 8.2 and later.

Kindlt refer to the link below for more information:

https://www.se.com/ww/en/product-range-presentation/62919-ecostruxure%E2%84%A2-power-monitoring-expert​

Schneider Electric USA

Attachment(s)
PM5000_Series_LE_6.0.1.11_ENG.zip [7.37 MB]