{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can you use the same relays for fixed and withdrawable breakers and will the fault/arc flash times be the same?
Issue:
use of relay for fixed breakers

Product Line:
Harmony Electromechanical Relays

Environment:
Relays – Interface, Control and Measurement

Resolution:
Yes, you can use the same relay as long as it fits within the means of the low voltage box of the switchgear. Fixed switchgear will traditionally have a smaller low voltage box that could restrict the size of your relay, but not the capability of the relay. For example, a 751-amp arc flash relay can be used in either fixed or withdrawable switchgear.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: