{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the difference in an NSX cord and a circuit breaker ULP cord?
Product Line:
Circuit Breakers

Resolution:
Besides the various lengths, the cable itself is the same. It consists of a 4-wire cable with an RJ45 jack at one end. The difference is what is terminated at the other end of the cable.

NSX Cord (example - see S434201 picture below)
The NSX cord has an RJ45 jack at one end, and 4 wires terminated into a small terminal block on the other end. This is used with Powerpact H, J, and L breakers. If the terminal block is not needed, it can be removed.

Circuit Breaker ULP Cord (example - see LV434195 picture below)
The circuit breaker ULP cord has an RJ45 jack at one end, and at the other end, the 4 wires are ready to be connected into screw terminals of an accessory such as a communication module. This is used with Powerpact P, R, and Masterpact NT and NW breakers to connect the BCM to the communication network.


NSX cord ULP cord

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: