{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Programming an Enersure BCPM with a New IP Address
Issue
How to modify an IP address already set in Enersure BCPM?

Product Line
Enersure BCPM

Environment
Netcfg utility

Cause
Network changes

Resolution
In order to modify the IP address there is a need for Netcfg utility.  The attachmet includes this utility along with the instructions in PDF format.

1. Double click on the Netcfg.exe to open the tool.
2. Click on the 'Discover' button.  This will detect all Enersure devices on the network.
3. Highlight the device in question.  The current IP address will be shown.
4. Modify the IP address, subnet mask, gateway.
5. Click on the 'Set' button.
6. Enter 'password' when prompted for password.
 

Schneider Electric USA

Attachment(s)
NetcfgUtility.7z [1.14 MB]