Issue:
Are the FFTK and HHTK the same thing?
Product Line:
Powerpact Circuit Breaker Test Sets
Resolution:
S33595
The S33595 Full Function Test Set is used to test Powerpact M, P and R circuit breakers, with these trip units:
Basic: ET 1.0M, ET 1.0I, ET 1.0
Standard: Micrologic 2.0, 3.0, 5.0
Ammeter: Micrologic 2.0A, 3.0A, 5.0A
Power: Micrologic 5.0P, 6.0P
Harmonic: Micrologic 6.0P, 6.0H
STRV00910
The STRV00910 UTA Tester is used to test Powerpact H, J and L electronic circuit breakers, with these trip units:
Standard: Micrologic 3.2, 3.2S
Ammeter: Micrologic 5.2A, 6.2A
Energy: Micrologic 5.2E, 6.2E
See the attached files to compare the differences between the two test sets.
Are the FFTK and HHTK the same thing?
Product Line:
Powerpact Circuit Breaker Test Sets
Resolution:
S33595
The S33595 Full Function Test Set is used to test Powerpact M, P and R circuit breakers, with these trip units:
Basic: ET 1.0M, ET 1.0I, ET 1.0
Standard: Micrologic 2.0, 3.0, 5.0
Ammeter: Micrologic 2.0A, 3.0A, 5.0A
Power: Micrologic 5.0P, 6.0P
Harmonic: Micrologic 6.0P, 6.0H
STRV00910
The STRV00910 UTA Tester is used to test Powerpact H, J and L electronic circuit breakers, with these trip units:
Standard: Micrologic 3.2, 3.2S
Ammeter: Micrologic 5.2A, 6.2A
Energy: Micrologic 5.2E, 6.2E
See the attached files to compare the differences between the two test sets.
Released for:Schneider Electric USA