{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
ION7400 default template in missing in Designer
Issue
When attempting to open an ION 7400 meter in Designer, a "Default template is missing" message appears and all of the modules are arranged as follows:


Product Line
ION 7400

Cause
The registry is pointing to the following folder for the default ION7400 node diagram for Designer: <PME installation folder>\system\Diagrams\nd\7400_FAC-PQ-61850-4WYE_V1.0.1
The default diagram in that folder is supposed to have the same name as the folder.  However, in PME 8.1, it got installed under the name 7400_FAC-PQ-61850-4WYE_V1.0.0.cfg (i.e. it ends in 1.0.0 instead of 1.0.1).

Environment
Configuring ION 7400 meter in Designer

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).

1) Navigate to <PME installation folder>\system\Diagrams\nd\7400_FAC-PQ-61850-4WYE_V1.0.1
2) Open the folder and rename the default ION7400 node diagram from 7400_FAC-PQ-61850-4WYE_V1.0.0.cfg to be 7400_FAC-PQ-61850-4WYE_V1.0.1.cfg
3) Find the name of the device that user has given to ION 7400 meter and locate the node diagram within the <PME installation folder>\config\diagrams\nd folder
4) Delete any node diagrams that were created for the ION7400 Device within the <PME installation folder>\config\diagrams\nd folder
5) Reopen the ION7400 Device in Designer so that Designer can generate a new node diagram for it.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.