{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Powerpact R frame lug wire binding screw torque
Product Line:
Circuit Breakers

Resolution:
For unit mounted Powerpact R frame circuit breakers, the torque of the AL2500RK lug wire binding screw is 46 lb-ft (550 lb-in) (62 N-m).

For I-line mounted Powerpact R frame circuit breakers, the torque of the AL1200R53K, AL1200R53TK, and CU1200R53K lug wire binding screw is 37.5 lb-ft (450 lb-in) (50 N-m).



Schneider Electric USA