{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
When testing with the FFTK, the trip indication on a Micrologic 6.0A/P/H trip unit is Ig, regardless of the function being tested
Issue:
Full function test kit shows ground fault regardless of the test being performed

Product Line:
Molded Case and Air Circuit Breakers

Resolution:
This is because of the way the FFTK tests the trip unit. The FFTK detects a trip by the drop in supply voltage (since the trip unit diverts it all to the trip solenoid). With PI testing, as with in-service, when the breaker trips, the signal goes away and the indication is correct. But with the FFTK, the test signal can still be applied after the trip unit initially sends the trip signal causing multiple protection functions to react. The Ig light is last to react and therefore is the light that is latched on.
If the FFTK says the breaker passes, it passes.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.