{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Unable to ping an ION8650 over a cellular modem
Issue
The ION8650 has a valid Cellular IP address, but ping, tracert and telnet commands are unsuccessful.

Product line
ION8650 with cellular modem

Cause
The ION8650 cellular modem doesn’t allow pings or any other commands/protocol excepts for the ones defined under Cellular Protocol Options within the meter’s communication setup. These protocols can be either ION, Modbus TCP and/or DNP 3.0.

Resolution
To test the Cellular modem’s connectivity, Use the appropriate software platform that will allow you to communicate over the defined protocol. Refer to FA277446 for further information.

Schneider Electric USA