{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: Differences between Homeline™ (HOM) plug-on neutral and non plug-on neutral panels and breakers
Issue:
Differences between HOM Plug-On Neutral and Non Plug-On Neutral Panels and Breakers
 
Product Line:
Load Centers
 
Resolution:
The difference in the load centers is that the neutral bar on the plug-on neutral panels will extend to the bottom of the interior, and will have spaces in between the screws for the breakers to attach to. The neutral bar on the non plug-on neutral panels will be much shorter.

The plug-on neutral breakers will not have a pigtail, and will have a rejection feature on the bottom to restrict them to only plug-on neutral panels. The non plug-on neutral breakers will have a pigtail and will not have the rejection feature (as the breakers can be used in both styles of panels).

See video below for more information.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: