{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the part number for the replacement cover for a Masterpact NW circuit breaker?
Product Line:
Circuit Breakers

Resolution:
For Masterpact NW circuit breakers, the part numbers for the replacement covers are shown below. These covers include the red reset button.
Note that the serial number of the existing breaker will be required when the order is placed.

S47939
  • IEC Fixed and Drawout
  • UL / ANSI Fixed

S47939U
  • UL / ANSI Drawout (non-limiter)

S47939L
  • UL / ANSI Drawout (limiter L, L1)

Schneider Electric USA