{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the Part Number for the ION6200 Remote Display?
Issue
The remote display for the ION6200 needs to be replaced.

Product Line
ION6200

Environment
Remote Display Hardware

Cause
Updated part numbers for remote displays and cables are required.

Resolution
S620DR1 = Standard remote display with 14ft cable
S620DN1 = MegaWatt option remote display with 14ft cable (for MegaWatt option or Transducer meter base)

*Note: Part numbers start with 'P' for Canada (i.e. P620DR1). Please see attached part number guide for Canadian part numbers and options.

The remote display cables can be ordered separately. Part numbers for US and Canada are as follows:
- P620C1 for 14ft
- P620C2 for 6ft

Please note that the 30ft remote display cable (P620C3) and the 3ft remote display cable (P620C4) are obsolete.

Schneider Electric USA

Attachment(s)
ION6200_RemoteDisplayPN.PNG.png [75.49 KB]