{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the CH362AWC, series F07 (may be shown as F7)?
Issue:
Design repair parts

Product Line:
Canadian Heavy Duty Safety Switches

Resolution:
The repair parts for the CH362AWC, Series F07 (F5) are as follows. No other parts are available.
Line Base Assembly -4056603850  (1 required; arc suppressor assembly not included)
Load Base Assembly - 4056604050 (1 required)
Line and Load Base Mounting Screw - 4020515102 (3 for line and 2 for load)
Arc Suppressor Assembly - 4056635550 (1 required)
Arc Suppressor Mounting Screw - 4020514501 (1 required)
Handle assembly - 4056663550 (should also replace handle gasket 4056603101)
Switch Mechanism - 4056787350 (should also replace interlock gasket 4056603201 and the washer 2360200008)
Linkage Assembly - 4056787050 (linkage between the switch mechanism and the receptacle)
Lock Plate - 4056672101
Lock Plate mounting screws - 2299940562 (2 required)
Lug Kit - CL0306F (includes all line and load lugs)
Fuse Pullers - FPK0610
Receptacle - 2541002311 (This is ONLY the receptacle that attaches to the bottom of the safety switch, it does not include the wires or any other part)
Receptacle Mounting Screws - 4510280101 (4 required)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: