undefined undefined
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the single phase ratings for Schneider Electric LK4MU3N disconnects?
Issue:
What are the single phase ratings for Schneider Electric Non-Fused disconnects?

Product Line: 
Operating Mechanisms and Disconnect Switches

Environment:
Operating Mechanism and Disconnect Switches

Cause:
​Customer would like to use the LK4 non fused disconnect line on single phase voltage

Resolution:
Our LK4 non-fused devices up to 200A have the below single phase ratings (Compact units: LK4DU3CN-LK4JU3CN will have this marking on their performance label)
   1ph -Max HP rating* 
Schneider P/NRating@120VAC@240VAC@480VAC
LK4DU3CN30A2510
LK4GU3CN60A51025
LK4JU3CN100A51025
LK4JU3N100A 10 
LK4MU3N200A 10 
LK4QU3N400AN/AN/AN/A
LK4SU3N600AN/AN/AN/A
LK4TU3N800AN/AN/AN/A
LK4UU3N1000AN/AN/AN/A
LK4WU3N1200AN/AN/AN/A
















*For any single phase ratings outside of the above table scope. Devices will be amperage rated only.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more