{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the NEMA Rating on I-Line II Busway?
Issue:
What is the Nema rating on  I-Line II Busway?

Product Line:
I-Line busway sold and supported in the USA.

Environment:
Specification

Cause:
Product Features

Resolution:
I-Line II busway is available as Indoor and Outdoor Rated products. Busway products are designed per UL857 and IEC529 and are not assigned NEMA ratings.
Below are the offered ratings. See attached IP Chart.
Indoor Rated Offerings: (Plug-In and Feeder Busway)
Standard Indoor (IP40)
M Type Drip Resistant (IP42)
M54 Type Splash Resistant (IP54)

Outdoor Rated Offerings: (Feeder Busway Only)
Standard outdoor (IP65) UL approved.
Standard outdoor (IP66) UL approved for Indoor installations only, IEC approved for Outdoor Installations.


Schneider Electric USA

Attachment(s)
Degrees of Protection, SE-X0004-EN[1].pdf [65.72 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top