{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the "Grid Reconnect Delay" standard for an XC680-NA?
Issue:
Grid Reconnect Delay period for XCNA inverter?

Product Line:
XCNA inverter

Environment:
Applications that use any XCNA inverter

Cause:
What is the grid reconnect delay

Resolution:
This setting is based on the utility region.  For IEEE 1547, the grid reconnect delay is 300 seconds.

Note:This only takes effect if there is a grid error, this does not apply to start/stop if there are no errors.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more