{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: How does the LK225ANHOM neutral/ground lug install into Homeline plug-on neutral load centers?
Issue:
Product Design Features

Product Line:
Homeline Load Centers

Resolution:

The LK225ANHOM branch neutral/ground lug can ONLY be installed in Series S04, 150-225amp Max. Homeline Load centers and Combination Service Entrance Devices(CSED) with Homeline Plug-On Neutral interiors, Series M01..
The LK225ANHOM branch neutral/ground lug will install on one of the branch neutral bars on the load center or CSED interior and will mount under two(2) wire binding screws as per the instructions that come with the kit.
The LK225ANHOM and will accept (1) #4 -  300kcmil Al/Cu wire.

The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below Safety Information that is located in the instructions BEFORE working on any electrical equipment.

A PDF copy of the complete instructions is attached below the video.

Danger label pic

Make sure to turn OFF ALL Power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
1) Once all Safety steps are followed, begin the kit installation by following the instructions.
2) Remove Cover from load center or CSED.
3) To install the neutral lug kit into the load center, refer to (a) and (b) below and mount ONLY in the location shown in the instructions.
a) Homeline load centers and CSED panels using Homeline interiors
b) Loosen the 4th and 6th neutral bar wiring binding screws on either side of the interior. See Figure 1 in the instructions.
NOTE: the Neutral lug is mounting to the top of a small Plate that has projections(or Tangs) on one side of the the plate.
4) Insert the projections (or Tangs) of the neutral lug mounting plate in the holes of the neutral bar under the screws that were loosened in step 3.
5) Torque the two wire binding screws to 35 lb-in( 4 N-m) to secure the neutral lug to the neutral bar.
6) Use the appropriate neutral wire size for the application and torque the wire binding screw for the neutral wire to 250 lb-in (28.3 N-m)

NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.

Schneider Electric USA

Attachment(s)
LK225ANHOM instructions.pdf [401.68 KB]