Search FAQs
What is the part number for the end tap box for Busway part AF2520G10ST and all other lengths?
Issue:
What is the part number for the end tap box for the aluminum feeder and plug in type 2000A Busway rated 3 phase 4 wire?
Like a AF2520G10ST?
Product Line:
busway
Environment:
I-line II
Cause:
Part selection
Resolution:
The part number is AF2520GETBMB. Change the A to a C for copper.
What is the part number for the end tap box for the aluminum feeder and plug in type 2000A Busway rated 3 phase 4 wire?
Like a AF2520G10ST?
Product Line:
busway
Environment:
I-line II
Cause:
Part selection
Resolution:
The part number is AF2520GETBMB. Change the A to a C for copper.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: