{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is there a CM2000 adapter plate for the PM5500 series devices?

Issue
Customer needs to replace the CM2000 meter with a PM5500 meter.

Product Line
CM2000, PM5500

Environment
PM5500 Commissioning

Cause
The opening of the CM2000 is too large for the PM5500 to be installed.

Resolution
The part number for the mounting adapter is CM2TOPM5K (not available in Canada).
Description: CM2 TO METSEPM5563RD Remote Display Meter Retrofit Assembly. Includes meter and Assembly fully pre-wired for direct CM2 Replacement.

This is a custom 'standardized' solution developed by the Schneider Electric USA Digital Power Team, which is a standard part for the US only. For Canadian customers, they will be required to purchase the PM5K meter and a retrofit plate (APPMCM2). 

For additional information on the installation of this product please reach out to the Customer Projects & Services manager, Craig Carpenter.

Schneider Electric USA

Attachment(s)
CM2TOPM5K_SUBMITTAL_DWGS.pdf [868.52 KB]
APPMCM2.pdf [53 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: