{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: How do you wire a 9070T transformer with the voltage code D20?
Issue:
Wiring a  9070T transformer with the voltage code D20?

Product Line:
Control power transformer (CPT)

Environment:
9070 T CPT

Cause:
Wiring assistance

Resolution:
If wiring for 208V - 115V bring the 208V to H1 and H2 and the output to X1 and X2. Ground X2 per the NEC code to be the neutral. 
If wiring for 230V - 115V bring the 230V to H1 and H3 and the output to X1 and X2. Ground X2 per the NEC code to be the neutral.
If wiring for 460V - 115V bring the 460V to H1 and H4 and the output to X1 and X2. Ground X2 per the NEC code to be the neutral.

When grounding per the NEC code, LAHJ will also need to be consulted as well.
 
The following video illustrates the terminal identification markers on 9070 Type T industrial control power transformer (CPT) wiring diagram labels:

 

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range: