{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
DC Voltages with ABL8REM24050, ABL8REM24030, ABL7RP1205, and ABL7RP4803
Issue:
Can the Phaseo Optimum units use a DC input voltage?

Product Line:
Universal power supplies

Environment:
Phaseo Power Supply

Cause:
Product Application

Resolution:
These units are capable of utilizing a DC input voltage.  However, it should be noted that the product itself will not have a DC specification on the product label.  This is because the DC input voltages are not included in the cULus, cCSAus, and TUV certifications.  The acceptable voltages are shown in the instruction sheet for the product and are specified below:

ABL7RP1205 - Compatible with 110 to 220 Vdc
ABL7RP4803 - Compatible with 110 to 220 Vdc
ABL8REM24050 - Compatible with 110 to 220 Vdc
ABL8REM24030 - Compatible with 110 to 220 Vdc

Schneider Electric USA