{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is there a Class 9422 variable depth operating mechanism for the Powerpact B Frame breakers?
Issue:
Option for Class 9422 Variable-Depth Operating Mechanism for the Powerpact B Frame breakers.

Product Line:
Variable-Depth Operating Mechanism

Resolution:
The catalog number is 9422RB1. This does not include the 9422 handle operator. This operating mechanism is for 2P and 3P Powerpact B frame breakers. All circuit breaker operating mechanisms are suitable for either right- or left-hand flange mounting and are convertible on the job. The variable mounting depth range is 149 - 451 mm (5.88 - 17.75 in). For more information, see the instruction bulletin, NVE52882.

Note: Class 9422 operating mechanisms are not available for 4-pole B-frame breakers.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: