Search FAQs
What is the largest branch breaker available on a Speed-D switchboard with an I-line interior configuration?
Issue:
Need the highest amp breaker that can go in a Speed D board's I-line distribution section.
Product Line:
Class 2710 Switchboards
Environment:
Speed-D Interiors
Cause:
Need to know if a 600 A feeder breaker can be installed
Resolution:
The largest breaker that can be installed on the right is a 400A LA or LH frame and the largest breaker on the left is 250A J-frame. The I-line section of Speed-D boards has 27" of mounting space.
Need the highest amp breaker that can go in a Speed D board's I-line distribution section.
Product Line:
Class 2710 Switchboards
Environment:
Speed-D Interiors
Cause:
Need to know if a 600 A feeder breaker can be installed
Resolution:
The largest breaker that can be installed on the right is a 400A LA or LH frame and the largest breaker on the left is 250A J-frame. The I-line section of Speed-D boards has 27" of mounting space.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: