{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: How to install the LV426906 fixed OFF position handle padlock attachment on the PowerPacT B frame circuit breaker
Issue:
How do you install the LV426906 padlock device on a B-frame breaker?

Product Line:
Circuit Breakers

Resolution:
Make sure the breaker is in the off position, and slide the tab on the padlock attachment into the slot above the handle on the breaker. Then, screw the attachment onto the breaker with the provided screw. For more installation information, see the attached installation bulletin and video below:

Schneider Electric USA

Attachment(s)
B Frame Fixed Padlock Attachments.pdf [1.46 MB]