{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is a ground bail used for in Metal Clad VR breaker Switchgear ?
Issue:
What is the purpose of a ground bail in Metal Clad VR breaker Switchgear ?

Product Line:
Metal Clad VR Breaker 

Environment:
Product Features 

Cause:
Clarification

Resolution:
The ground bails are a grounding device used in switchgear for hooking the ground cables to and is considered a SIMPLE MANUAL ground-device per IEEE C37.20.6 when used with grounding cables.  A simple manual device has two sets of terminals and has manual operated hookstick-operable connections between the phases and the ground bus
Ground Bails from Switchboard

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
move-arrow-top