Search FAQs
What is the purpose of the Qwik-Grip Load Centers?
Issue:
Load Center features
Product Line:
QO and Homeline Load Centers
Resolution:
Square D plug-on neutral load centers with Qwik-Grip wire management system speeds up wire installation by not having to remove knockouts, install wire connectors and pull wires through knockouts. Qwik-Grip inserts are factory installed and ready to wire. Simply snap off a Qwiklet tab, and slide in the wire.
To learn more about the plug-on neutral QO and Homeline Qwik-Grip load centers see the Qwik-Grip Load Center Brochure.
Load Center features
Product Line:
QO and Homeline Load Centers
Resolution:
Square D plug-on neutral load centers with Qwik-Grip wire management system speeds up wire installation by not having to remove knockouts, install wire connectors and pull wires through knockouts. Qwik-Grip inserts are factory installed and ready to wire. Simply snap off a Qwiklet tab, and slide in the wire.
To learn more about the plug-on neutral QO and Homeline Qwik-Grip load centers see the Qwik-Grip Load Center Brochure.
Released for:Schneider Electric USA
Attachment(s)
Explore more
Range:
Explore more
Range: