Issue:
Is there a weight limit for the Ceiling Mounting Brackets, CMB or 7400CMB for EX Transformers?
Product Line:
Low Voltage Transformers
Environment:
7400CMB22K
Cause:
Product Features
Resolution:
The largest Ceiling Mounting Bracket for EX Transformers, 7400CMB22K can hold up to maximum of 1300 pounds.
Is there a weight limit for the Ceiling Mounting Brackets, CMB or 7400CMB for EX Transformers?
Product Line:
Low Voltage Transformers
Environment:
7400CMB22K
Cause:
Product Features
Resolution:
The largest Ceiling Mounting Bracket for EX Transformers, 7400CMB22K can hold up to maximum of 1300 pounds.
Released for:Schneider Electric USA
Issue:
Is there a weight limit for the Ceiling Mounting Brackets, CMB or 7400CMB for EX Transformers?
Product Line:
Low Voltage Transformers
Environment:
7400CMB22K
Cause:
Product Features
Resolution:
The largest Ceiling Mounting Bracket for EX Transformers, 7400CMB22K can hold up to maximum of 1300 pounds.
Is there a weight limit for the Ceiling Mounting Brackets, CMB or 7400CMB for EX Transformers?
Product Line:
Low Voltage Transformers
Environment:
7400CMB22K
Cause:
Product Features
Resolution:
The largest Ceiling Mounting Bracket for EX Transformers, 7400CMB22K can hold up to maximum of 1300 pounds.
Released for:Schneider Electric USA