Search FAQs
What is the difference between a PK18GTA and PK18GTAL?
Issue:
What does the "L" mean on part number PK18GTAL?
Environment:
QO load center ground bar
Cause:
Clarifying feature differences
Resolution:
The PK18GTA has the same features as the PK18GTAL except that the PK18GTAL has an extra lug. It is a standard PK18GTA with a 1-4/0 Al/Cu additional lug.
What does the "L" mean on part number PK18GTAL?
Environment:
QO load center ground bar
Cause:
Clarifying feature differences
Resolution:
The PK18GTA has the same features as the PK18GTAL except that the PK18GTAL has an extra lug. It is a standard PK18GTA with a 1-4/0 Al/Cu additional lug.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: