{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Video: What filler plate is used and how does it install to fill the main circuit breaker opening in QO and Homeline, low amp, convertible main load center covers?

Article available in these languages: Spanish

Issue:
Product Design Features

Product Line:
QO and Homeline Load Center

Resolution:
The low amp (100-125 A max.) QO (single phase) and Homeline load centers that use a QOM1 main breaker will use the filler plate part number QOM1FP.

The attached video is ONLY to supplement the INSTRUCTIONS that come with the kit. PLEASE make sure to read the instructions and all the below safety information that is located in the instructions BEFORE working on any electrical equipment.

A PDF copy of the complete instructions is attached below the video.

Danger image

Make sure to turn OFF ALL power supplying the equipment and verify the power is OFF using a properly rated voltage sensing device, BEFORE working on or with electrical equipment.
1) Once all safety steps are followed, begin the installation of the main breaker opening filler plate by following the instructions.
2) Install the filler plate (A) from the front of cover (B) by pressing into place as shown
NOTE: PLEASE READ ALL INSTRUCTIONS AND SAFETY INFORMATION THAT COME WITH THE KIT AND NEVER WORK ON ENERGIZED EQUIPMENT.

Schneider Electric USA

Attachment(s)
QOM1FP Instructions.pdf [41.73 KB]