{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How Can a 120V Single Phase Panelboard be ordered?
Issue:
Customer requires a 120V single phase panel, not 120/240V.

Product line:
Circuit breaker panelboards sold and supported in the USA.

Environment:
Application

Cause:
Customer requirement

Resolution:
In product selectors, select a 240V 1Ph 3W. panelboard.  Add feed through lugs.  In special pricing, instruct the plant to jumper A & C phases, remove the C phase main lug,
and re-label the panelboard as 120V 1 P 2W.  Use $0, Tag # DIGEST

Schneider Electric USA