{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What timing type is the RUW101MW timer?
Issue:
What timing functions does the RUW101MW timer module have?

Product Line:
Relays and Timers

Environment:
Zelio Relays and Timers

Cause:
Product Features

Resolution:
The selectable timing functions are as follows: on-delay timer, interval timer, repeat cycle timer/start on-delay, repeat cycle timer/starting off-delay, off-delay timer, one-shot timer, timing on de-energization
See attached for information on how to set the dip-switches on the device for each function, as well as timing diagrams with more information.

Schneider Electric USA

Attachment(s)
DIA3ED2090304EN-RPM-US FINAL LO-RES.pdf [2.4 MB]