{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What are the repair parts for the H365NDS, series E5 (or E05) heavy duty safety switch?
Issue:
Repair parts

Product Line:
HD Safety Switch

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 4055218851 (3 required; arc suppressor assembly included)
Load base assembly - 4055219050SEL (3 required)
Arc suppressor assembly - 4051270850 (3 required)
Lug Assembly - 4025113650 (1 required per base assembly)
Line base phase insulator - 4051201401 (2 required)
Load base phase insulator - 4055219101 (1 required)
Line & load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051219151
Mounting screw and washer for Handle assembly - 2140122242 (screw; 2 required) and 2370100220 (washer; 2 required)
Door Thumb Screws and retainers - S1A99898 (thumb screw; 2 required) and 4405043301 (retainer; 2 required)
Handle knob kit - 4028343550
Cross Bar Insulator - 4055217701
Dust Shield - 4055215701
Cross Bar Insulator - 4055217801
Solid Neutral Assembly - 4055225250SEL (can also use H600SN)
Bonding Strap assembly - 4028337950SEL

Schneider Electric USA

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: