{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How to adjust the set points of the 9012 Type G Pressure Switches
Issue:
9012G Pressure switches set up

Product Line: 
Pressure, Vacuum, and Float Switches

Environment:
Pressure Switches

Resolution:
The pressure switch is factory set to the operating setpoints marked on the outside of the switch housing. Before readjusting the switch, cycle it to determine the actual operating setpoints. 

Non-Adjustable Differential
(GDW, GDWM, GEW, GEWM, GFW, GFWM

The range adjustment nut (H) or knob (C) adjusts both setpoints by the same amount. To adjust the setpoints:

1. Place a flat-blade screwdriver in a slot of the range adjustment nut. 
2. To raise the setpoints, rotate the nut to the left (CCW). To lower the setpoints, rotate the nut to the right (CW). 

Adjustable Differential
(GAW, GAWM, GBW, GBWM, GCW, GCWM)

The range adjustment nut or knob determines the decreasing setpoint.The adjusting screw (J) determines the increasing setpoint. To adjust the set points:

1. Adjust the decreasing setpoint
(see Steps 1–2 above).

2. To raise the increasing setpoint, turn the adjusting screw to the
right (CW). To lower the increasing setpoint, turn the adjusting screw to the left (CCW). This adjustment does not affect the decreasing setpoint.

Schneider Electric USA

Attachment(s)
65013-008-90.pdf [4.24 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top