Issue:
Load shows negative in the System Status page.
Product Line:
XW+ Inverter/Charger, XW+ system control panel
Environment:
Applications that use a system control panel(part#865-1050 or 865-1050-01)
Cause:
System status screen is showing load as negative
Resolution:
If the load shows a negative symbol, then that means that the unit is in AC coupled mode. AC coupled is selling power to the grid from the AC output of the inverter. This means that there are grid tie or micro inverters connected to the subpanel which will cause current to flow in reverse from output to input which will then show the load as negative. See image below as an example.
![]()
Load shows negative in the System Status page.
Product Line:
XW+ Inverter/Charger, XW+ system control panel
Environment:
Applications that use a system control panel(part#865-1050 or 865-1050-01)
Cause:
System status screen is showing load as negative
Resolution:
If the load shows a negative symbol, then that means that the unit is in AC coupled mode. AC coupled is selling power to the grid from the AC output of the inverter. This means that there are grid tie or micro inverters connected to the subpanel which will cause current to flow in reverse from output to input which will then show the load as negative. See image below as an example.
Released for:Schneider Electric USA
Issue:
Load shows negative in the System Status page.
Product Line:
XW+ Inverter/Charger, XW+ system control panel
Environment:
Applications that use a system control panel(part#865-1050 or 865-1050-01)
Cause:
System status screen is showing load as negative
Resolution:
If the load shows a negative symbol, then that means that the unit is in AC coupled mode. AC coupled is selling power to the grid from the AC output of the inverter. This means that there are grid tie or micro inverters connected to the subpanel which will cause current to flow in reverse from output to input which will then show the load as negative. See image below as an example.
![]()
Load shows negative in the System Status page.
Product Line:
XW+ Inverter/Charger, XW+ system control panel
Environment:
Applications that use a system control panel(part#865-1050 or 865-1050-01)
Cause:
System status screen is showing load as negative
Resolution:
If the load shows a negative symbol, then that means that the unit is in AC coupled mode. AC coupled is selling power to the grid from the AC output of the inverter. This means that there are grid tie or micro inverters connected to the subpanel which will cause current to flow in reverse from output to input which will then show the load as negative. See image below as an example.