Search FAQs
Are the voltage indicators field installable on a safety switch?
Issue:
Product Design Features
Product Line:
Heavy Duty Safety Switches
Environment:
Safety Switch Accessories
Resolution:
Voltage monitors are NOT available for field installation on ANY safety switch. They are only available factory installed on certain heavy duty and double throw switches. They are NOT available for general duty switches.
1) For heavy duty, they can ONLY be factory installed on the 30 - 1200 A, NEMA Type 12 or 4X stainless steel switches
2) For double throw, they can ONLY be factory installed on the 30 - 200 A, NEMA Type 12 or 4X stainless steel switches
To ADD them to any of the available safety switches, it requires the use of the Product Selector System for ordering.
Product Design Features
Product Line:
Heavy Duty Safety Switches
Environment:
Safety Switch Accessories
Resolution:
Voltage monitors are NOT available for field installation on ANY safety switch. They are only available factory installed on certain heavy duty and double throw switches. They are NOT available for general duty switches.
1) For heavy duty, they can ONLY be factory installed on the 30 - 1200 A, NEMA Type 12 or 4X stainless steel switches
2) For double throw, they can ONLY be factory installed on the 30 - 200 A, NEMA Type 12 or 4X stainless steel switches
To ADD them to any of the available safety switches, it requires the use of the Product Selector System for ordering.
Released for:Schneider Electric USA
Explore more
Range:
Explore more
Range: