{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How many auxiliary switches can I put in a Powerpact H, J, or L circuit breaker with electronic trip unit?
Issue:
How many OF Aux Contacts will fit in an H, J or L breaker with Electronic Trip Unit?
How many SD Alarm Switches will fit in an H, J or L breaker with Electronic Trip Unit?
How many SDE Overcurrent Trip Switches will fit in an H, J or L breaker with Electronic Trip Unit?

Product Line:
Circuit Breakers

Resolution:
For H, J or L circuit breaker with electronic trip unit, the number of aux contacts, alarm switches, or overcurrent trip switches that can be installed depends on which communications accessories are already in the breaker. The below picture shows how many OF, SD or SDE contacts can be installed in the breaker. This assumes that the breaker does not have a motor operator, or an SDx module.



Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: