{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What determines the fuse clip voltage for Fusible Combination Starters?
Issue:
What determines the fuse voltage for Fusible Combo Starter?

Product Line:
NEMA Contactors and Starters

Environment:
8538/8539 Type S Combination Starters

Resolution:
The type of combination starter will indicate what fuse clip voltage is included. When selecting from the digest, or in the product selector, the motor voltage selected determines the fuse clip type. A 208-204V motor will give a 250V fuse. 480-575V motor will have a 600V fuse.

Schneider Electric USA