undefined undefined
{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
How do key interlocks work?
Issue:
How are Kirk key interlocks (or other brands) used to interlock circuit breakers?

Product Line:
MCCB

Resolution:
If you have two circuit breakers transferring load between a utility and main (for example) in the absence of synchronizing equipment, it is acceptable to only have one on at a time; never both.  
To accomplish this, you would have a keylock in both breakers, both keyed the same, and only one key. Without the key, the breaker is locked OFF, so only the one breaker with the key can be turned ON. This prevents both sources from feeding the load simultaneously.

If you have three breakers in a main-tie-main arrangement, it is acceptable to have any two breakers on at a time.  So each breaker has a lock, all keyed alike, and you are provided two keys. The breaker without a key cannot be turned on but the others can, satisfying the need.

Other keying schemes are possible; these illustrate the principle.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.