{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Is there an enclosure available for Powerpact H frame breakers with ELM150HD earth leakage modules?
Issue:
Is there a suggested enclosure size for breakers with ELM150HD, earth leakage module?

Product Line:
Circuit Breaker

Resolution:
No, we do not offer an enclosure that would accept Powerpact H frame breaker with an ELM150HD.  However the instruction bulletin, 48041-089-01, lists recommend minimum size for customer sourced enclosures.
Minimum recommended size for standard 80% rated breakers would be 18.13 in. H x 8.63 in. W x 4.13 in. D. For 100% rated breakers, 62 in. H x  22 in. W x  14 in. D.

Schneider Electric USA