{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
GSAH36F, GSAH60F, GSAH120F, GSAH144F, GSAH180F Why are these numbers not recognized on Schneider tools.
Issue:
Customers are trying to order the cable operator kits but the numbers on Digest 177 are not valid.

Product Line:
UL98 IEC Style Disconnect Switches

Environment:
LK4 Non Fussible and GS2 Fusible Switches

Resolution:
These numbers are misprints on the hard copy of the Digest 177 page 8-9, table 8.38. The correct part numbers are as follows:
GS2AH36F - 36 in. Cable Operator Kits for GS2 Switches, 200 A and Below
GS2AH60F - 60 in. Cable Operator Kits for GS2 Switches, 200 A and Below
GS2AH120F - 120 in. Cable Operator Kits for GS2 Switches, 200 A and Below
GS2AH144F - 144 in. Cable Operator Kits for GS2 Switches, 200 A and Below
GS2AH180F -  180 in. Cable Operator Kits for GS2 Switches, 200 A and Below

Schneider Electric USA