{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the difference between the shunt XF coil and the shunt XF-COM coil?
Issue:
XF & XFCOM technical differences

Product Line:
Molded Case Circuit Breaker

Resolution:
The shunt close (XF) remotely closes the circuit breaker if the spring mechanism is charged. Once voltage is present on the coil, it will close the breaker.
The shunt close with communications (XF-COM) needs a third hot wire from a different power source. This needs constant control voltage and must be connected via the circuit breaker communication module (BCM). it allows the closing of the breaker through comms.

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: