Issue:
Part number for a shunt trip accessory for a PA, PC, PE or PX breaker
Product Line:
Molded Case Circuit Breakers
Resolution:
The following are the catalog numbers for shunt trip kits for series 4 and higher PA, PC, PE, and PX breakers. Note that some or all of these may be obsolete:
PA11042 (24 Vac)
PA11021 (120 - 240 Vac)
PA11037 (277 Vac)
PA11027 (24 Vdc)
PA11028 (48 Vdc)
PA11029 (125 Vdc)
PA11030 (250 Vdc)
Part number for a shunt trip accessory for a PA, PC, PE or PX breaker
Product Line:
Molded Case Circuit Breakers
Resolution:
The following are the catalog numbers for shunt trip kits for series 4 and higher PA, PC, PE, and PX breakers. Note that some or all of these may be obsolete:
PA11042 (24 Vac)
PA11021 (120 - 240 Vac)
PA11037 (277 Vac)
PA11027 (24 Vdc)
PA11028 (48 Vdc)
PA11029 (125 Vdc)
PA11030 (250 Vdc)
Released for:Schneider Electric USA