{}

Our Brands

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the torque requirement for cable, busbar, and compression lug connection for the Powerpact L frame breaker?
Issue:
What is the torque requrement for the Powerpact L frame breaker lug wire binding screw, lug mounting screw, busbar connection, and compression lug?

Product Line:
Circuit breakers

Resolution:
Torque requirements are as follows:
Lug wire binding screw for lug kits AL400L61K3, AL600LS52K3, CU600LS52K3, AL600LF52K3, CU600LF52K3:  442 lb.-in. or 50 N-m.
Lug wire binding screw for CU400L61K3:   31 N-m or 275 lb.-in.
Lug mounting screw:  327 lb-in (37 N•m)
Rear Connectors:  177 lb.-in (20 N-m)
Busbar:  442 lb-in / lbs-in. (50 N•m)
Compression lug:  442 lb-in. (50 N•m)

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
move-arrow-top